Replace a CP600 control panelPermalink

Control panels are maintenance free. Spare parts are not available and repair is not permitted. If a control panel becomes inoperable, it must be replaced. An operation manual is included with the new unit.

For instructions on how to transfer the runtime to a new control panel and how to load projects to a new control panel, refer to the ‎⮫ Panel Builder manual.

The procedure for changing from a CP600 device to a CP600 device of the 2nd generation is described in the application example ‎⮫ Converting a CP600 project. A description of the differences between both device variants can also be found in this application example.